Cookies on the OMEGA websites
We use cookies on this website, these cookies are essential for the website to work correctly.If you continue without changing your settings, we'll assume that you are happy to receive all cookies on this website.To find out more information about these cookies please click here.
CLOSE
Basket  |  Contact  |  Help  | 
Holland07077 03815
International+31 (0) 7077 03815

Your Source for Process Measurement & Control

Signal Conditioning

Introduction to Signal Conditioners

A signal conditioner is a device that converts one type of electronic signal into a another type of signal. Its primary use is to convert a signal that may be difficult to read by conventional instrumentation into a more easily read format. In performing this conversion a number of functions may take place. They include:

Amplification

When a signal is amplified, the overall magnitude of the signal is increased. Converting a 0-10mV signal to a 0 -10V signal is an example of amplification.

Electrical Isolation

Electrical isolation breaks the galvanic path between the input and output signal. That is, there is no physical wiring between the input and output. The input is normally tranferred to the output by converting it to an optical or magnetic signal then it is reconstructed on the output. By breaking the galvanic path between input and output, unwanted signals on the input line are prevented from passing through to the output. Isolation is required when a measurement must be made on a surface with a voltage potential far above ground. Isolation is also used to prevent ground loops.

Linearization

Converting a non-linear input signal to a linear output signal. This is common for thermocouple signals.

Cold Junction Compensation

Used for thermocouples. The thermocouple signal is adjusted for fluctuations in room temperature.

Excitation

Many sensors require some form of excitation for them to operate. Strain gages and RTDs are two common examples.

Choose the right signal conditioner for your application

Top
DIN Rail Mount DIN Rail Mount
As the name implies, a DIN rail mount signal conditioner mounts on a DIN rail bracket. DIN rail conditioners are very popular in industrial applications since they provide a rugged mounting format for either a few or a large number of signal conditioners.
Backplane Mount Conditioners Backplane Mount Conditioners
Certain signal conditioners can also be mounted on a common backplane. The backplane style provides the advantage of all output signals being accessible through a single common connnector. The backplane style signal conditioners are often used with data acquisition systems since a single cable can connect multiple conditioners to a data acquisiton device.
Digital Signal Conditioners Digital Signal Conditioners
Digital conditioners are one of the more recent developments in signal conditioners. The output of a digital signal conditioner is converted to a digital format such as RS232, RS485 or even Ethernet. Digital signals have several advantages over analog signals. They provide a high degree of immunity from electrical noise, they can also support extended transmission distances and are easily connected to a computer. With an ethernet output, the input signal can be read across an entire network or even across the internet if so configured.