Cookies on the OMEGA websites
We use cookies on this website, these cookies are essential for the website to work correctly.If you continue without changing your settings, we'll assume that you are happy to receive all cookies on this website.To find out more information about these cookies please click here.
CLOSE
Basket  |  Contact  |  Help  | 
Holland 07077 03815
International+31 (0) 7077 03815

Calibrator

Introduction to process and temperature instrument calibration

A calibrator is an equipment used to adjust an instrument accuracy, often associated with a specific application. The most sophisticated industrial equipment will not be very useful unless it is calibrated. Through calibration, adjustments made to a piece of equipment ensure that it performs as expected—that it can be relied on to deliver predictable, accurate results that meet quality standards.

Simply defined, calibration is the process of adjusting a device to meet manufacturer’s specifications. Calibration is sometimes also defined as the issuing of data, including a report or certificate of calibration, that assures an end user of a product’s conformance with specifications, and perhaps also with external guidelines, such as those of the International Organization for Standardization, whose ISO 9001 standards, for example, set worldwide specifications for business sectors. A company follows these standards to ensure that its products and/or services gain acceptance among suppliers and customers. This second definition of calibration is more properly referred to as certification.

Most instruments and sensors are designed to meet certain accuracy specifications; the process of adjusting an instrument to meet those specifications is referred to as calibration. The device used to calibrate other instruments is known as a calibrator. Calibrators vary in form and function depending on the instruments with which they are designed to work.

A sofisticated lab calibrator with very high accuracy

Learn more about calibrator

What Is NIST Traceability?


The National Institute of Standards and Technology (NIST), part of the U.S. Department of Commerce, oversees the development of measurement standards and technology consistent with the International System of Units (SI). NIST is also charged with imparting these standards to the American system of measurements through calibrations and other services. To help U.S. industry meet international standards, NIST provides, among other programs, laboratory accreditation that enables a business to establish traceability of measurement results.

The Calibration Process

A company with equipment needing calibration may send it to a metrology/calibration laboratory, where a skilled technician will either bring it up to specifications or confirm that it already meets them, using measurement/test instruments that must themselves meet strict calibration requirements. All or part of the components used in an industrial process can be calibrated. A temperature calibration, for example, could involve a probe alone, an instrument alone, or a probe connected to an instrument (a system calibration). Adjustments made during calibration must fall within certain tolerances. Such tolerances represent very small, acceptable deviations from the equipment’s specified accuracy.

How often should an instrument be calibrated?

The manufacturer usually does the initial calibration on its equipment. Subsequent calibrations may be done in-house, by a third-party lab, or by the manufacturer. The frequency of recalibration will vary with the type of equipment. Deciding when to recalibrate a flowmeter, for example, depends mainly on how well the meter performs in the application. If liquids passing through the flowmeter are abrasive or corrosive, parts of the meter may deteriorate in a very short time. Under favorable conditions, the same flowmeter might last for years without requiring recalibration. As a rule, however, recalibration should be performed at least once a year. Of course, in critical applications frequency will be much greater.

What Is Involved in a Typical Calibration?

A weighing system serves well in illustrating general principles of calibration. Archimedes and Leonardo Da Vinci used the positioning of calibrated counterweights on a mechanical lever to balance and thereby determine unknown weights. A variation of this device uses multiple levers, each of a different length and balanced with a single standard weight. Later, calibrated springs replaced standard weights.

The introduction of hydraulic and electronic (strain gage-based) load cells represented the first major design change in weighing technology. In today’s processing plants, electronic load cells are preferred in most applications. To check if transducers and load cells are functioning properly, the user must answer the following: Does the weight indication return to zero when the system is empty or unloaded? Does the indicated weight double when the weight doubles? Does the indicated weight remain the same when the location of the load changes (uneven loading)? If the answers are yes, the cells and transducers are probably in good condition.

Sign up for the omega.co.uk e-mail newsletter! Click here for help finding your calibrator!

Choose the right calibrator

Top
BB701 Black Body temperature Calibrator for infrared sensor cablibration Black Body Calibrators
A black body is used for calibrating infrared thermometers. They typically consist of a target plate that has a very high emisivity. The temperature of the target plate can be controlled to very tight tolerances. To calibrate and infrared pyrometer, the pyrometer makes a measurement of the the target plate. The controlled temperature of the plate is compared with the IR sensor reading. The pyrometer is then adjusted until the the difference is minimal. The high emissivity of the target plate minimizes emissivity errors.
Block Calibrators Block temperature Calibrators
Block Calibrators are used for calibrating temperature probes. They contain a metal block that can be heated to a precise temperature. Temperature probes can be inserted into the block and the measured temperature of the probes can be compared with the controlled temperature of the blocks. Since temperature probes generally don't have any adjustments, this is really verification process rather than a true calibration.
The CL125 Thermocouple Simulator allows you to create different temperature signals Simulators and Signal References
When calibrating an instrument, such as a panel meter or temperature controller, it is necessary to input a precise known electrical signal. The instrument's display or output value can then be adjusted to match the input signal. a signal reference is used to generate the precision signal. Signal references are available as voltage references, current references and frequency references. When working with an instrument that reads a sensor, such as thermocouple, a special type of signal reference, called a simulator is used. The simulator can accurately reproduce a sensor output. Many signal references and simulators can not only generate signals but read them as well.
Fluidized Sand Bath Temperature Probe Calibrators Fluidized Sand Bath Calibrators
Fluidized baths provide safe, rapid heat transfer and accurate temperature control, enabling you to efficiently and safely calibrate and maintain temperature sensitive instruments. The principle of fluidization occurs when a gas usually low pressure air or nitrogen flows upward through a partially-filled chamber or retort of dry, inert particles of aluminum oxide. The gas flows at a low velocity, which sets the particles in motion, separates them, then suspends them to a stable level to give the particles the appearance of turbulence quite similar to the state of boiling liquid. Besides circulating and flowing like a liquid, fluidization solids exhibit excellent heat transfer characteristics. Temperature probes inserted into the bath come to a consistent, stable temperature very quickly.
ice point Calibration Reference Chambers ice point™ Calibration Reference Chambers
ice point™ calibration reference chambers employ thermoelectric cooling elements to produce a very precise stable 0°C reference chamber. The reference chamber can be used for calibrating temperature probes but they are also commonly used in simulating a thermocouple signal for the calibration and verification of instruments that read thermocouples.

Frequently Asked Questions

Top

Why Is Calibration Important?

On April 12, 1934, an anemometer on the summit of Mount Washington in New Hampshire measured the highest surface wind speed ever recorded: 231 miles per hour. The Mount Washington anemometer, which had been calibrated in 1933, was recalibrated after the world record measurement, and it proved to be accurate. When a typhoon hit Guam in December of 1997, the record seemed to be broken — an anemometer at an American air force base recorded a wind gust of 236 mph. That reading, however, did not stand because the National Climate Extremes Committee judged the Guam anemometer unreliable. To metrology experts, the survival of the old record was an object lesson in the importance of calibration. A footnote: wind speeds greater than 231 mph are believed to have occurred in tornadoes, but no documentation device has yet withstood such extremes. Contrary to rumor, the Mount Washington anemometer did not blow away during the 1934 storm. Today, it resides in the mountain’s Observatory Summit Museum.

For a more down-to-earth example of what happens when calibration gets short shrift, one need look no further than the “oven temperatures may vary” statement on the cooking instructions of frozen food. The reason for the caveat is that most household ovens are never recalibrated after they leave the factory. Consumers apparently can live with this margin of error, but it is a different story for manufacturers. For a company to be ISO 9001-compliant, equipment calibration is required. Rules alone, however, do not explain why the best companies recognize the importance of doing calibration correctly and frequently.

Considering the benefits in quality, productivity, and revenue that a well-designed calibration program can realize, costs are reasonable. Although small calibration tasks can be adequately performed in-house using off-the-shelf calibrators, most medium-to-large companies that view calibration as a high priority opt for the services of an independent metrology/calibration lab. A very large company might consider investing in automated equipment intended for conducting many daily calibrations, but such equipment—the same kind used by independent labs—is expensive, and it requires skilled technicians. If gaining certification from some outside calibration authority is also necessary, this adds to costs

We noticed you are from the US. Visit your local site for regional offers and live support.